Part Number: TMS320F28379D
Tool/software: TI C/C++ Compiler
Hi,
I am trying to make large arrays of variables as buffers which I need to download to the PC in debug mode. For this I am using the RAM GS8-15. I am using the :>> so that I can split the ebss section in multiple RAM blocks. However, the entire ebss section gets stored in the largest memory block greatly reducing the array size that I can use. I am not sure what is going wrong.
Section definitions that I am using for the data.
.stack : > RAMM1, PAGE = 1
.ebss : >> RAMD0D1|RAMGS0GS1|RAMGS89101112131415, PAGE = 1
.econst : > RAMD0D1|RAMGS2, PAGE = 1
Any suggestions for a more efficient way to create memory buffers for downloading signals from the DSP?
Thank you,
Aditya