Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi.
I stumbled in a situation where my RAM and FLASH code, started by emulator and loaded in CPU1+CLA and CPU2+CLA, running well but unfortunately when I loading it in FLASH_STANDALONE mode CPU1/CPU2 code stuck! I tried to understand this strange behavior because I loaded a previous FLASH STANDALONE code and this works well. Recently, my actual code is raised in dimension (.text extension in .cmd linker file) while it was debugged in RAM. So, I decided to find the new CPU1 FLASH STAND_ALONE stuck condition by the use of GPIO Test Point motion. Anyway, I follow this post
and I realized that my C2000Ware support was crossed. Now my code using the new “F2837xD_Ipc_Driver_Util.c” with few TI changing;
The salient beginning structure in my code, excluded comment, is:
CPU1:
void main(void)
{
InitSysCtrl_CPU1();
#ifdef _STANDALONE
#ifdef _FLASH
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else
IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif
#endif
#ifdef _FLASH
InitFlash();
#endif
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
EALLOW;
PieVectTable.ADCA1_INT = &ADCA_ISR_CPU1;
PieVectTable.ADCD1_INT = &ADCD_ISR_CPU1;
PieVectTable.TIMER0_INT = &AD7490_SPI_timer0_isr;
PieVectTable.EPWM1_INT = &Loop_Epwm1_ISR_CPU1;
PieVectTable.CANA0_INT = &CanA0_isr;
PieVectTable.CANB0_INT = &CanB0_isr;
IER |= M_INT1;
IER |= M_INT3;
IER |= M_INT9;
EDIS;
PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
PieCtrlRegs.PIEIER9.bit.INTx5 = 1;
PieCtrlRegs.PIEIER9.bit.INTx7 = 1;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieCtrlRegs.PIEACK.all = 0xFFFF;
EINT;
ERTM;
// *** WATCHDOG SETTINGS ***
DisableDog(); // JUST DO IT in InitSysCtrl_CPU1();
System_Config_CPU1();
Init_Vars_CPU1();
// Spin here until CPU02 is ready
while(IPCRtoLFlagBusy(IPC_FLAG17) == 0);
// DEBUG CODE IN FLASH STAND_ALONE MODE
do
{
DELAY_US(100);
GpioDataRegs.GPCCLEAR.bit.GPIO76 = 1;
DELAY_US(100);
GpioDataRegs.GPCSET.bit.GPIO76 = 1;
}
while(1); // END DEBUG CODE
// BACKGROUND LOOP
for(;;)
{ …
void System_Config_CPU1(void)
{
Init_GPIO_CPU1();
Setup_PWM_CPU1();
EALLOW;
ClkCfgRegs.XCLKOUTDIVSEL.bit.XCLKOUTDIV = 2; // CPLDCLK = 50MHz
EDIS;
InitCpuTimers();
Setup_Timer0_CPU1();
SPI_A_Init();
SPI_C_Init();
AD7490_Init();
MCP23S17_Init(MCP23S17_ALL_PORT_IN, MCP23S17_ALL_PORT_OUT, 0x00, 0x00);
DMA_Init_CPU1();
Init_Uart_A();
Init_Uart_B();
CANInit(CANA_BASE);
CANInit(CANB_BASE);
Setup_CAN_A();
Setup_CAN_B();
CANGlobalIntEnable(CANA_BASE, CAN_GLB_INT_CANINT0);
CANIntEnable(CANA_BASE,CAN_INT_IE0 | CAN_INT_STATUS);
CANGlobalIntEnable(CANB_BASE, CAN_GLB_INT_CANINT0);
CANIntEnable(CANB_BASE,CAN_INT_IE0 | CAN_INT_STATUS);
DAC_Init(DACA);
DAC_Init(DACB);
DAC_Init(DACC);
I2CB_Init();
ConfigureADC_CPU1();
Setup_ADC_CPU1();
// Setup Shared Global RAM
Setup_SharedRAM();
Cla1Regs.MIER.all = 0;
EALLOW;
CpuSysRegs.PCLKCR0.bit.CLA1 = 1;
EDIS;
CLA1_ConfigMemory();
CLA1_Init();
}
void Setup_SharedRAM(void)
{
// Give CPU02 Memory Access to GSRAM15
do
{
EALLOW;
MemCfgRegs.GSxMSEL.bit.MSEL_GS15 = 1;
EDIS;
}
while(MemCfgRegs.GSxMSEL.bit.MSEL_GS15 == 0);
}
CPU2:
#ifdef _FLASH
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadSize;
extern Uint16 RamfuncsRunStart;
#endif
void main(void)
{
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
InitSysCtrl_CPU2();
#ifdef _FLASH
InitFlash();
#endif
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
EALLOW;
PieVectTable.ADCC1_INT = &ADCC_ISR_CPU2;
PieVectTable.EPWM7_INT = &Loop_Epwm7_ISR_CPU2;
IER |= M_INT1;
IER |= M_INT3;
EDIS;
PieCtrlRegs.PIEIER1.bit.INTx3 = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
PieCtrlRegs.PIEIER3.bit.INTx7 = 1;
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieCtrlRegs.PIEACK.all = 0xFFFF;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// Wait until Shared RAM is available
while(MemCfgRegs.GSxMSEL.bit.MSEL_GS15 == 0);
// Unblock CPU1 Code Execution
do
{
IPCLtoRFlagSet(IPC_FLAG17);
} while(IpcRegs.IPCFLG.bit.IPC17 == 0);
// DEBUG CODE IN FLASH STAND_ALONE
do
{
GpioDataRegs.GPCSET.bit.GPIO81 = 1; // TP E38
DELAY_US(100);
GpioDataRegs.GPCCLEAR.bit.GPIO81 = 1;
DELAY_US(100);
} while(1); // END DEBUG CODE
System_Config_CPU2();
Init_Vars_CPU2();
// *** WATCHDOG SETTINGS ***
DisableDog();
// BACKGROUND LOOP
for(;;)
{
In conclusion, if I load CPU1 FLASH STAND_ALONE code and CPU2 FLASH code and then using script “EMU Boot Mode Select -> EMU_BOOT_FLASH” whit CPU2/CPU1 run command, I didn’t see CPU1&CPU2 TP toggling: I have introducing an infinite loop to force TP toggling to observe FLASH STAND_ALONE code activity also whit emulator disconnected and DIP switch BM0&BM1 setted to 1 (3V3 verified whit multimeter/oscilloscope). If I stopped CPU1 code I see it looping in IPCBootCPU2(), specifically:
//
// Wait until CPU02 control system boot ROM is ready to receive
// CPU01 to CPU02 INT1 interrupts.
//
do
{
bootStatus = IPCGetBootStatus() & C2_BOOTROM_BOOTSTS_SYSTEM_READY;
} while ((bootStatus != C2_BOOTROM_BOOTSTS_SYSTEM_READY));
If I stop CPU2 and force IPCBOOTSTS = 2, than CPU1 and CPU2 starting to move on !
Why Boot ROM sequence didn’t change CPU2 IPCBOOTSTS correctly ?
Thanks for your support.
Diego