Part Number: TMS320F28377D
We are trying to program the C2000 series TMS320F28377D delfino Microcontroller, but there is error in programming and we cannot find the solution. The error log file is attached please check.
Please check the log file and revert ASAP.
Thanks & Regards
Rahul Ponarkar
[3/4/2019, 5:54:03 PM] [INFO] C28xx_CPU2: GEL Output: Memory Map Initialization Complete [3/4/2019, 5:54:03 PM] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete [3/4/2019, 5:54:05 PM] [INFO] C28xx_CPU2: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed. [3/4/2019, 5:54:05 PM] [INFO] C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed. [3/4/2019, 5:54:08 PM] [ERROR] C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.100.0) [3/4/2019, 5:54:08 PM] [ERROR] C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0xC095) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.100.0) [3/4/2019, 5:54:08 PM] [ERROR] C28xx_CPU1: Unable to determine target status after 20 attempts [3/4/2019, 5:54:08 PM] [ERROR] C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging [3/4/2019, 5:54:10 PM] [ERROR] C28xx_CPU2: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.100.0) [3/4/2019, 5:54:10 PM] [ERROR] C28xx_CPU2: Error: (Error -1135 @ 0x3FEC52) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.100.0) [3/4/2019, 5:54:10 PM] [ERROR] C28xx_CPU2: Unable to determine target status after 20 attempts [3/4/2019, 5:54:10 PM] [ERROR] C28xx_CPU2: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0) [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: File Loader: Memory write failed: Unknown error [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug. [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x5D200@Program: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug. [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected [3/4/2019, 5:54:28 PM] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected