This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F2808: Move from code generation tools V5.1.2 to V18.1.1LTS on F2808

Part Number: TMS320F2808

Tool/software: TI C/C++ Compiler

Hi expert,

My customer would like to move their F2808 project from old code generation tool (V5.1.2) to some new one (V18.1.1LTS). They are afraid of the differences between the two could cause some error in code execution. Do you have any advice or tips for doing this kind of transfer?

Thanks

Sheldon

  • No compiler vendor can guarantee a new release will never have a problem.  That said, it is not common.  TI compilers are tested with a number of commercial test suites.  Further, we have tests that are developed from the bug reports which are filed.  We run those tests to be sure the problems we fix do not return.  More information can be found in the article Compiler Validation.

    Thanks and regards,

    -George