This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-HV-1PH-DCAC: Project Created through Solution Adapter does not allow modifiable options...

Part Number: TIDM-HV-1PH-DCAC
Other Parts Discussed in Thread: C2000WARE, POWERSUITE

Tool/software: Code Composer Studio

I have generated a project using the following...  

Resource Explorer -> C2000Ware_DigitalPower_SDK - v1.02.00.00 -> Power Suite -> Solution Adapter -> Single Phase Inverter: Voltage Source  ->  TMS320F28004x

I was expecting the main.cfg (PowerSuite) page to have modifiable options, but most are still grayed out.   If  I open the compensation designer and try to "Save COMP", this also fails.  

  • After looking into this a while, I have been able to make the project modifiable, but would still like confirmation from TI...
    I had to make a change to Kit.xml file:
    From
    <ProjectNonModifiable>1</ProjectNonModifiable>
    to
    <ProjectNonModifiable>0</ProjectNonModifiable>

    I also had to add an empty file called .cookie to the project to keep this from going back to 1 when opening the main.cfg powersuite file.

    This problem exists for all versions and processors related to this kit.
  • Wayne,

    Thanks for pointing out this issue. I have filed a bug against this item.

    Regards,
    Ozino