Hi,
I am trying to design a USB communication circuit based on the TMS320F28377D.
So I am looking at the USB circuit of the F28379D ControlCARD.
In the attached circuit, The 5V level signals are connected to the GPIO ports of 28X chip through USB-VBUS, USB_FLT lines.
As far as I know, the 28X chip's GPIO port allowable voltage range is from GND to VDDIO (3.3V).
Is it okay to design the circuit similar to the F28379D ControlCARD?
I would like to know if there is a reference circuit that connects the USB Type-A connector to the USB communication port of the TMS320F2837x chip.