Other Parts Discussed in Thread: C2000WARE
Q: What is depletion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
A:
Note: This answer applies to devices with F05 flash. Refer to: [FAQ] F05 Flash: Which C2000 devices have "F05 flash"?
Also refer to this FAQ: https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/757586
If the erase operation is interrupted and not allowed to complete, the device may become depleted. This is a state of over-erase. When this happens, the device may then begin to fail to erase at all. The Flash API has a depletion recovery function to try to recover flash that has been "over-erased". Refer to the Flash API documentation for a specific device for more details: C2000Ware_\libraries\flash_api\\docs\
For more F05 related FAQs refer to [FAQ] F05 Flash: Frequently Asked Questions