Part Number: TMS320F28027
I am trying to blink LED with every press of button. I have attempted to write the code but I am missing something somewhere. Please help me figure out.
#include "DSP28x_Project.h"
interrupt void xint1_isr();
void main()
{
InitSysCtrl();
/*Interrupt config*/
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW;
PieVectTable.XINT1 = &xint1_isr;
PieCtrlRegs.PIECTRL.bit.ENPIE =1;
PieCtrlRegs.PIEIER1.bit.INTx4 = 1;
PieCtrlRegs.PIECTRL.bit.PIEVECT= 0x0D46;
IER |= M_INT1;
EINT;
/*Input GPIO*/
//GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO12 = 0;
GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 0;
GpioIntRegs.GPIOXINT1SEL.bit.GPIOSEL =12;
XIntruptRegs.XINT1CR.bit.POLARITY = 0;
XIntruptRegs.XINT1CR.bit.ENABLE =1;
/* LED Blink*/
// GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
while(1);
}
interrupt void xint1_isr()
{
GpioDataRegs.GPATOGGLE.bit.GPIO0 = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}