Part Number: TMS320F28033
Other Parts Discussed in Thread: SM73201
Tool/software: Code Composer Studio
SIR,
THANKS FOR REPLY.
sir my code is working. . when i has PRESSED switch (SW1) and probed at TEST POINT (TP17) ARC is generating so it is OK.
but when i measure same signal after CAPACITOR (C75) it is not transferring to ADC pin
what i have done is, i has removed this capacitor (C75) and i am sure that i has already R63 AND C78 RC filter is available on ADC pin so i would not pic up a noise.
now i did not understand why this capacitor needed to be removed.?
what happen if actual ARC is generating then i needed the this capacitor?
regards,
vishal.