This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28035: Using 28035 serial chip for UL1998 Standard

Genius 3095 points

Part Number: TMS320F28035

Tool/software: Code Composer Studio

Dear Team:

I am a developer of MCU, recent days ,I am using 28035 serial MCU for UL1998 Standard certification.The following are some microelectronic fault check:

1.CPU Check, To confirm PC/SP and other special register works normally

2、RAM check, to complete read and write all address of ram to make sure ram works fine

3、FLASH check, to confirm there is no unnormal  rectification  in flash range of code

It is very kind of you to provide some suggestions or some technical documents,thanks

Best Regards