Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Hi friends,
I am doing can interface in TMS320F28377D Dev Board Rev1.1 and I have taken the reference code from C2000.
The example code can_external_loop-back.c file i modified as per my requirement I have to communicate with SOC board.
SOC board having two on board transceiver so I am using one for TMS320f28377D(I have taken the TX and RX wires from the transceiver to my board pin 80 and 82) other for SOC board.
But while transmitting their receiving end very first time no data is available.After 28377D reset SOC is able receive the datas
but only once next time SOC only reading constant those datas.
While I am modified as only receiver i am not getting the interrupt in ISR?
I read status reg LEC is coming 7 and sometimes 1.How it is happening?
Can anybody please help me how to find out the issue?
Reagrds,
Ashru