This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28027: are I2c interface lines SDA/SCL driven by 5V Logic or 3.3V ?

Part Number: LAUNCHXL-F28027


Hello,

I am using the f28027 i2c to communicate with a S2GO PRESSURE DPS310 but this device has a maximum rating of 4 V...that's why i have to ensure that no voltage applied to any of the device's pins
exceeds the absolute maximum rating of 4 V or it might be damaged.

So is the  LAUNCHXL-F28027 a 5 V logic board? does (SDA/SCL) pins outputs 3.3v or 5v !!? Thanks.

Regards,