Tool/software: Code Composer Studio
the default InstaSpin project inside MotorWare was originally developed for driving the DRV8312 using the 3-PWM mode (not 6-PWM),
•• Can DRV8312 generate OUTA,OUTB, and OUTC like this picture as datasheet?
and what the CC project for that to build on the KIT DRV8312-69M-KIT, in other word
I need the code to compile on CC to generate trapezoidal signal like below
or the following if 100% internal PWM