This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Modbus Communication

Part Number: LAUNCHXL-F28069M

Hello,

I am working on modbus communication. My F28069M is master and MFM meter is slave. Modbus communication is working fine, F28069M sends query and meter sends response. All the work I am doing in CCS.

But the problem is that I want to read voltage from meter (230V), and the data which I am receiving in SCI buffer is 0x80BC from meter. That data is not equal to 230V. Is it the data format issue or something going wrong. I have executed the modbus communication in Matlab also (PC master and meter slave). I have sent the read command for holding registers and input registers. I the meter's response is as below:

Those values are also not equal to 230V, but the meter is working well, then what is the issue. 

Regards,

Nisha