This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Need part number for the connector for the TMS320F28379D controlCARD R1.3

Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMDSHSECDOCK, C2000WARE

We are planning to use the TMS320F28379D controlCARD R1.3.

Where can I find the part number or the connector type for this controller card.

Thanks for the help

Roger

  • Roger,

    there are two part numbers, they can be found in the BOM for the TMDSHSECDOCK located at: "C:\ti\c2000\C2000Ware_1_00_06_00\boards\ExperimenterKits\DockingStation_ HSEC_120or180pin\R5_0" within C2000Ware.

    1. HSEC8-160-01-L-DV-A-BL
    2. HSEC8-130-01-L-DV-A

    The first pin of the second connector is 21mm OC from the last pin of the first connector. Please see the attached JPG. Regards,

    Cody