Part Number: TMS320F28069F
I've been tried to write flash memory.
I referred to TI flash memory writer. And my application is based on windows MFC.
so,my serial writer function is like this...
-----------------------------------------------------------------------
UINT Serial_Flash_Programmer(LPVOID lpData)
{
PointerToDev* thInfo = (PointerToDev*)lpData;
CProdcutManagerView* pThread = thInfo->pView;
CMainFrame* pMain = thInfo->pMain;
int devNo = thInfo->deviceNo;
int iExitCode = 0;//_tmain
CString g_strComPort;
CString g_strBaudRate;
DCB port;
//CString str;
CString g_strAppFile(_T(""));
CString g_strKernelFile(_T(""));
g_strKernelFile = pThread->GetKernelTxtFile(); // Kernel file
g_strAppFile = pThread->GetAppTxtFile(); // App file
if (initFlashProgrammer(pThread, devNo, g_strKernelFile, g_strAppFile)==0)
{
return 0;
}
HANDLE commPortFile = NULL;
if (initComPort(pThread, devNo, &port, &commPortFile) == 0)
{
...//errorHandling...
return 0;
}
FILE *Kfh;
Kfh = openKernel(pThread, devNo, g_strKernelFile);
if (Kfh == NULL)
{
...//errorHandling...
return 10;
}
FILE *Afh;
Afh = openApp(pThread, devNo, g_strAppFile);
if (Afh == NULL)
{
...//errorHandling...
return 10;
}
if (setKernelAutoBaud(pThread, commPortFile, devNo) < 0)
{
...//errorHandling...
return(12);
}
TRACE(_T("Kernel AutoBaud Successful\n"));
writeKernel(pThread, commPortFile, Kfh, devNo);
Sleep(1000);
if (setAppAutoBaud(pThread, commPortFile, devNo) < 0)
{
return(12);
}
if (writeApp(pThread, commPortFile, Afh, devNo) < 0)
{
return 12;
}
CloseHandle(commPortFile);
CString str;
...//successHandling...
pMain->PrintBuild(str);
return 0;
}
-----------------------------------------------------------------------
I've got some problem with writeApp(...).
When writeApp does some checksum test, endless 0-byte reading roof triggers.
Below is the part.
-----------------------------------------------------------------------
int writeApp(CProdcutManagerView* pThread, HANDLE targetBoard, FILE* AppFileHandle, int devNo)
{
...//preview is all passed processes...
int pos = 0;
while (1)
{
CString str;
fileStatus = fscanf_s(AppFileHandle, "%x ", &sendData[0]);
if (fileStatus == EOF)
break;
WriteFile(targetBoard, &sendData[0], 1, &dwWritten, NULL);
checksum += sendData[0];
// Get block size
// block size = targetBoard[0] + (targetBoard[1]<<8)
if (txCount == 0x00)
{
w_blockSize = sendData[0];
}
else if (txCount == 0x01)
{
byteData = sendData[0];
// form the wordData from the MSB:LSB
w_blockSize |= (byteData << 8);
}
txCount++;
//If the next block size is 0, exit the while loop.
if (w_blockSize == 0x00 && txCount > 1)
//handle file end
{
w_blockSize = 0x0000;
byteData = 0x0000;
//str.Format(_T("testing checksum :%d"), pos);
pThread->SetNotify(devNo, _T("Test passed."));
break;
}
// will execute when all the data in the block has been sent
else if (txCount == 2 * (w_blockSize + 3))
//handle block end
{
str.Format(_T("testing checksum :%d, send"), pos);
pThread->SetNotify(devNo, str);
doublewordReadCount = 0;
while (doublewordReadCount == 0)
{
ReadFile(targetBoard, &rcvData, 1, &doublewordReadCount, NULL);
}
doublewordReadCount = 0;
while (doublewordReadCount == 0)
{
ReadFile(targetBoard, &rcvDataH, 1, &doublewordReadCount, NULL);
}
//Ensure checksum matches
if (checksum != (rcvData | (rcvDataH << 8)))
{
TRACE(_T("chkSum(%x):%x"), checksum, (rcvData | (rcvDataH << 8)));
CloseHandle(targetBoard);
pThread->SetNotify(devNo, _T("Checksum error."));
return -1;
}
else
checksum = 0;
w_blockSize = 0x0000;
byteData = 0x0000;
txCount = 0x00;
}
// will execute when the flash kernel buffer is full (0x400 words == 0x800 bytes)
else if ((txCount - 6) % 0x800 == 0 && txCount > 6)
//handle kernel overflow
{
int retry = 0;
doublewordReadCount = 0;
rcvData = 0;
rcvDataH = 0;
while (doublewordReadCount == 0)
{
ReadFile(targetBoard, &rcvData, 1, &doublewordReadCount, NULL);
if (retry++ > 1000)
{
CloseHandle(targetBoard);
str.Format(_T("testing checksum :%d, txRead1:%d"), pos, txCount);
pThread->SetNotify(devNo, str);
return -1;
} }
...//remained process
return 1;
}
-----------------------------------------------------------------------
Result log is
"testing checksum :3515, txRead1 : 2054" and stopped.
I'm expecting upload app file is broken, but I'm not sure.
Because,
1. Some file is working well, but some file is not working.
2. All uploading with JTAG-writing is working well.
Can you check the file and what is the problem while uploading?
I'm waiting for the answer.