This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/C2000-CGT: TFT LCD TOUCH SCREEN DISPLAY

Part Number: C2000-CGT
Other Parts Discussed in Thread: BOOSTXL-SHARP128

Tool/software: Code Composer Studio

Which LCD display is good and compatible with C2000 launchpad?

TFT LCD display  interface with C2000 series to make user interface application.

  • Monali,

    Please see my reply in this thread: e2e.ti.com/.../740832

    short summary - the new BOOSTXL-SHARP128 will be compatible from a hardware perspective, but we have not provided drivers, nor have I seen others post any. That BoosterPack is only a display, no touch interface.

    Generally any display with a SPI, Parallel, I2C, CAN, or other interface should be compatible, but will need to be verified and tested beforehand.

    What other features do you need for your interface? You might also look at the MSP430 line with the built-in CapTouch interfaces if you do not need the real-time control features that the C2000 brings. www.ti.com/.../overview.html


    -Mark