Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
I am investigating the driverlib library for f28377d. I do not see any ipc library which makes the following initialization for the dual cpu flash boot.
#ifdef _STANDALONE #ifdef _FLASH //Send boot command to allow the CPU2 application to begin execution IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH); #else //Send boot command to allow the CPU2 application to begin execution IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM); #endif #endif
This part doesn't exist anf of the driverlib files. And also I don't see any example of dual flash boot project on the examples directory. Am I missing something or I need to implement this part on my own if I want to use driverlib?