This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: Unexpected behavior of Z1_BOOTCTRL

Part Number: TMS320F28075

Hello,

On our custom TMS320F28075 we need to move BOOTPIN1 to GPIO87.

First we checked board with default configuration, it starts normally from flash and then boots from SCI-A when the GPIO72 held low at power on.

We have programmed Z1OTP_BOOTCTRL, and verified Z1_BOOTCTRL register.

Now regardless of the GPIO87 status at power on, board always waits for SCI-A boot and never starts from flash.

We connected to board using JTAG and reprogrammed flash and it works by JTAG, after disconnecting JTAG we verified that nTRST is low from power on. But although GPIO87 is still boots only from SCI-A

What could be the reason for this?

With regards,

MHG