Part Number: TMS320F280049
Hello Support team.
I am reading TRM of F28004x.
And I understood that input data of DAC is DACVALS.
I understood that input data of ADC-A can be DACA_OUT of DAC-A. (Figure 12.-1)
Also without any configuration, ADC-A can input from DACA_OUT same as A0/B15/C15 ball.
I think that these (A0/B15/C15 and DACA_OUT) signals do not need to be control as pin mux.
But A0/B15/C15 is connected with outside module. (DC/DC, ABC and so on).
Sometime customer wants to check DAC/ADC module as self-checking. In this case ADC-A needs to get some data from DACA_OUT of DAC-A. But if external module is running and it is connected with A0/B15/C15, it is difficult to do self-checking.
I would like to know if C2000 can control A0/B15/C15 stop to input data from external module such as disabling.
Best Regards
KORO