This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Two resolver chip connection request

Part Number: TMS320F28377D


Hi, 

Customer has a request on traction project, inside two resolver chips (not PGA411) connection are needed. The reading of two resolver may be overlapped. 

In this case, we are thinking of two EMIF solution. Each C28x owns one EMIF. In this way, a lot of pins will be used, including the two boot pins.

So:

1) What's your suggestion, two EMIF or one EMIF by chip select?

2) The boot pins are used to connect to resolver chip. Do we need to change the boot pins to others? Or an external weak pull up?

3) Do we have any reference on the connection of EMIF and resolver chip?

Thanks a lot.

Br, Jordan