This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Generating a high frequency square wave

Part Number: TMS320F28377S

Hi,

I am running my system clock at 48 MHz which is fixed for my current design. I would like to generate and output a 10 MHz square wave which will act as a clock for one of the external payloads. I suppose bit-banging a GPIO using a timer interrupt may not be a good idea. Will ePWM be able to generate such high frequency or do I have to use some other method to generate? Just need a heads up towards right direction :)

Thanks and Regards,

Ankit