Part Number: C2000-GANG
Hi all,
For our product we have a royalty mode where Firmware is the control parameter. The Code is being manually flashed at the moment and adding a bootloader to the code is not feasible at this time. We wish to use C2000 Gang Programmer to do the same.
Please confirm if I can do the following with the C2000 Gang.
- We need to set the number of times the code needs to be flashed. Beyond this number, the instrument should not flash
- The Manufacturer must not be able to access the code. The code should be in internal memory and password protected
- Should be able to renew the licenses over Internet
We need to know these info before we go ahead and buy one.
Expecting a reply soon... thanks in advance.
Santhosh