Part Number: TMS320F28069
Hello,
yesterday I wanted to test the TMS320F28069 MCU on my developed circuit board.
I was able to establish a connection between my MCU and the PC. I did that by using the Test Connection button in the new Target Configuration menu.
After that I wanted to run my first code, but in the meantime a short circuit occurred in the 3,3V Power supply.
After some research I am quite sure, that the short circuit is inside the MCU.
Information:
- Every VDDIO-Pin is connected to 3,3V
- Every VDD and VDDIO is stabilized with a 2,2uF Capacitor.
- Every VSS is connected to Ground
- X1 and VREGENZ is connected to Ground
- The Short circuit has approximately 6,5 ohms
- The ground potential of the circuit board was floating, but nobody touched it (ESD).
Maybe the Problem is:
- I connected the X2-Pin via a 10k Resistor to Ground.
I want to to this to prevent floating Pins. The ground potential will be around -300 V (B6-Circiut).
I was not sure want will happen with floating pins and a ground potential around -300V, therefor I want to give it a defined potential.
- I did not connect VDDA and VREFHI and it was floating. VREFLO was connected to ground.
Questions:
- Is it possible to connect the X2-Pin via a 10k Resistor to Ground, or will it damage the MCU. Is this pin even floating or will it have a definite potential.
The dataset says to the X2-Pin: "If X2 is not used, it must be left unconnected."
- Does the floating VDDA and VREFHI pin cause the damage?
I could just test this, but I am running low on circuit brands and MCUs, so I just wanted to research the problem before testing. Also, I am not an original English speaker. If something isn't understandable, please tell me.
Thank you in advance :).