Part Number: F28M35H52C
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I am trying to write few commands to a device over I2C bus, I referred to the example code in C:\ti\controlSUITE\device_support\f28m35x\v220\F28M35x_examples_Master\i2c_loopback and tried editing it. I can not see any signal on SCL line and the code is stuck in
(I2CMasterBusy(I2C0_MASTER_BASE)
while loop.
Here is the full code i used.
//########################################################################### // FILE: i2c_loopback.c // TITLE: Example demonstrating a simple I2C message // transmission and reception. //########################################################################### // $TI Release: F28M35x Support Library v220 $ // $Release Date: Tue Sep 26 15:35:11 CDT 2017 $ // $Copyright: Copyright (C) 2011-2017 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### #include "inc/hw_memmap.h" #include "inc/hw_types.h" #include "inc/hw_i2c.h" #include "inc/hw_nvic.h" #include "inc/hw_sysctl.h" #include "driverlib/i2c.h" #include "driverlib/sysctl.h" #include "driverlib/gpio.h" #include "driverlib/flash.h" #include "utils/uartstdio.h" #include <string.h> //***************************************************************************** //! \addtogroup master_example_list //! <h1>I2C Master Loopback (i2c_master_slave_loopback)</h1> //! //! This example shows how to configure the I2C0 module for loopback mode. //! This includes setting up the master and slave module. Loopback mode //! internally connects the master and slave data and clock lines together. //! The address of the slave module is set in order to read data from the //! master. Then the data is checked to make sure the received data matches //! the data that was transmitted. This example uses a polling method for //! sending and receiving data. //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - I2C0 peripheral //! - GPIO Port B peripheral (for I2C0 pins) //! - I2C0SCL - PB2 //! - I2C0SDA - PB3 //! //! The following UART signals are configured only for displaying console //! messages for this example. These are not required for operation of I2C. //! - UART0 peripheral //! - GPIO Port E peripheral (for UART0 pins) //! - UART0RX - PE4 //! - UART0TX - PE5 //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - None. // //***************************************************************************** #ifdef _FLASH // These are defined by the linker (see device linker command file) extern unsigned long RamfuncsLoadStart; extern unsigned long RamfuncsRunStart; extern unsigned long RamfuncsLoadSize; #endif //***************************************************************************** // Number of I2C data packets to send. //***************************************************************************** #define NUM_I2C_DATA 3 //***************************************************************************** // Set the address for slave module. This is a 7-bit address sent in the // following format: // [A6:A5:A4:A3:A2:A1:A0:RS] // A zero in the "RS" position of the first byte means that the master // transmits (sends) data to the selected slave, and a one in this position // means that the master receives data from the slave. //***************************************************************************** #define SLAVE_ADDRESS 0x27 //***************************************************************************** // This function sets up UART0 to be used for a console to display information // as the example is running. //***************************************************************************** //void //InitConsole(void) //{ // // Enable GPIO port A which is used for UART0 pins. // // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); // // // Configure the pin muxing for UART0 functions on port A0 and A1. // // This step is not necessary if your part does not support pin muxing. // // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PE4_U0RX); // GPIOPinConfigure(GPIO_PE5_U0TX); // // // Select the alternate (UART) function for these pins. // // TODO: change this to select the port/pin you are using. // GPIOPinTypeUART(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5); // // // Initialize the UART for console I/O. // UARTStdioInit(0); //} //***************************************************************************** // Configure the I2C0 master and slave and connect them using loopback mode. //***************************************************************************** int main(void) { // unsigned long ulDataTx[NUM_I2C_DATA]; // unsigned long ulDataRx[NUM_I2C_DATA]; // unsigned long ulindex; // Disable Protection HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5; // Setup main clock tree for 75MHz - M3 and 150MHz - C28x SysCtlClockConfigSet(SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_2 | SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0x0F)); #ifdef _FLASH // Copy time critical code and Flash setup code to RAM // This includes the following functions: InitFlash(); // The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart // symbols are created by the linker. Refer to the device .cmd file. memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); // Call Flash Initialization to setup flash waitstates // This function must reside in RAM FlashInit(); #endif // The I2C0 peripheral must be enabled before use. SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0); // For this example I2C0 is used with PortB[3:2]. The actual port and // pins used may be different on your part, consult the data sheet for // more information. GPIO port B needs to be enabled so these pins can // be used. // TODO: change this to whichever GPIO port you are using. SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); // Configure the pin muxing for I2C0 functions on port B2 and B3. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. GPIOPinConfigure(GPIO_PB6_I2C0SDA); GPIOPinConfigure(GPIO_PB7_I2C0SCL); // Select the I2C function for these pins. This function will also // configure the GPIO pins pins for I2C operation, setting them to // open-drain operation with weak pull-ups. Consult the data sheet // to see which functions are allocated per pin. // TODO: change this to select the port/pin you are using. GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_6 | GPIO_PIN_7); // // Enable loopback mode. Loopback mode is a built in feature that is // // useful for debugging I2C operations. It internally connects the I2C // // master and slave terminals, which effectively let's you send data as // // a master and receive data as a slave. // // NOTE: For external I2C operation you will need to use external pullups // // that are stronger than the internal pullups. Refer to the datasheet for // // more information. // HWREG(I2C0_MASTER_BASE + I2C_O_MCR) |= 0x01; I2CMasterEnable(I2C0_MASTER_BASE); // Enable and initialize the I2C0 master module. Use the system clock for // the I2C0 module. The last parameter sets the I2C data transfer rate. // If false the data rate is set to 100kbps and if true the data rate will // be set to 400kbps. For this example we will use a data rate of 100kbps. I2CMasterInitExpClk(I2C0_MASTER_BASE, SysCtlClockGet( SYSTEM_CLOCK_SPEED), false); // // Enable the I2C0 slave module. This module is enabled only for testing // // purposes. It does not need to be enabled for proper operation of the // // I2Cx master module. // I2CSlaveEnable(I2C0_SLAVE_BASE); // // Set the slave address to SLAVE_ADDRESS. In loopback mode, it's an // // arbitrary 7-bit number (set in a macro above) that is sent to the // // I2CMasterSlaveAddrSet function. // I2CSlaveInit(I2C0_SLAVE_BASE, SLAVE_ADDRESS); // Tell the master module what address it will place on the bus when // communicating with the slave. Set the address to SLAVE_ADDRESS // (as set in the slave module). The receive parameter is set to false // which indicates the I2C Master is initiating a writes to the slave. If // true, that would indicate that the I2C Master is initiating reads from // the slave. I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, false); // // Set up the serial console to use for displaying messages. This is // // just for this example program and is not needed for I2C operation. // InitConsole(); // // Display the example setup on the console. // UARTprintf("I2C Loopback Example ->"); // UARTprintf("\n Module = I2C0"); // UARTprintf("\n Mode = Single Send/Receive"); // UARTprintf("\n Rate = 100kbps\n\n"); // Initialize the data to send. // ulDataTx[0] = 'I'; // ulDataTx[1] = '2'; // ulDataTx[2] = 'C'; SysCtlDelay(500000);//20ms delay I2CMasterDataPut(I2C0_MASTER_BASE, 0x30); I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_SEND); // Wait until master module is done transferring. while(I2CMasterBusy(I2C0_MASTER_BASE)) { } // // Initialize the receive buffer. // for(ulindex = 0; ulindex < NUM_I2C_DATA; ulindex++) // { // ulDataRx[ulindex] = 0; // } // // // Indicate the direction of the data. // UARTprintf("Transferring from: Master -> Slave\n"); // // // Send 3 pieces of I2C data from the master to the slave. // for(ulindex = 0; ulindex < NUM_I2C_DATA; ulindex++) // { // // Display the data that the I2C0 master is transferring. // UARTprintf(" Sending: '%c' . . . ", ulDataTx[ulindex]); // // // Place the data to be sent in the data register // I2CMasterDataPut(I2C0_MASTER_BASE, ulDataTx[ulindex]); // // // Initiate send of data from the master. Since the loopback // // mode is enabled, the master and slave units are connected // // allowing us to receive the same data that we sent out. // I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_SEND); // // // Wait until the slave has received and acknowledged the data. // while(!(I2CSlaveStatus(I2C0_SLAVE_BASE) & I2C_SCSR_RREQ)) // { // } // // // Read the data from the slave. // ulDataRx[ulindex] = I2CSlaveDataGet(I2C0_SLAVE_BASE); // // // Wait until master module is done transferring. // while(I2CMasterBusy(I2C0_MASTER_BASE)) // { // } // // // Display the data that the slave has received. // UARTprintf("Received: '%c'\n", ulDataRx[ulindex]); // } // // // Reset receive buffer. // for(ulindex = 0; ulindex < NUM_I2C_DATA; ulindex++) // { // ulDataRx[ulindex] = 0; // } // // // Indicate the direction of the data. // UARTprintf("\n\nTranferring from: Slave -> Master\n"); // // // Modify the data direction to true, so that seeing the address will // // indicate that the I2C Master is initiating a read from the slave. // I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, true); // // // Do a dummy receive to make sure you don't get junk on the first receive. // I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE); // // // Dummy acknowledge and wait for the receive request from the master. // // This is done to clear any flags that should not be set. // while(!(I2CSlaveStatus(I2C0_SLAVE_BASE) & I2C_SLAVE_ACT_TREQ)) // { // } // // for(ulindex = 0; ulindex < NUM_I2C_DATA; ulindex++) // { // // Display the data that I2C0 slave module is transferring. // UARTprintf(" Sending: '%c' . . . ", ulDataTx[ulindex]); // // // Place the data to be sent in the data register // I2CSlaveDataPut(I2C0_SLAVE_BASE, ulDataTx[ulindex]); // // // Tell the master to read data. // I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE); // // // Wait until the slave is done sending data. // while(!(I2CSlaveStatus(I2C0_SLAVE_BASE) & I2C_SLAVE_ACT_TREQ)) // { // } // // // Read the data from the master. // ulDataRx[ulindex] = I2CMasterDataGet(I2C0_MASTER_BASE); // // // Display the data that the slave has received. // UARTprintf("Received: '%c'\n", ulDataRx[ulindex]); // } // // // Tell the user that the test is done. // UARTprintf("\nDone.\n\n"); // // // Return no errors while(1); // return(0); }
Thanks.