Part Number: TMS320F28379D
Hi E2E team,
I am running sci_echoback example and with some minor modifications (GPIO9 and GPIO8 for RXD and TXD) I am seeing some garbage characters instead of alphabates.
The code I am running is here:
//########################################################################### // // FILE: Example_2837xDSci_Echoback.c // // TITLE: SCI Echoback. // //! \addtogroup cpu01_example_list //! <h1>SCI Echoback (sci_echoback)</h1> //! //! This test receives and echo-backs data through the SCI-A port. //! //! The PC application 'hyperterminal' or another terminal //! such as 'putty' can be used to view the data from the SCI and //! to send information to the SCI. Characters received //! by the SCI port are sent back to the host. //! //! \b Running \b the \b Application //! -# Configure hyperterminal or another terminal such as putty: //! //! For hyperterminal you can use the included hyperterminal configuration //! file SCI_96.ht. //! To load this configuration in hyperterminal //! -# Open hyperterminal //! -# Go to file->open //! -# Browse to the location of the project and //! select the SCI_96.ht file. //! -# Check the COM port. //! The configuration file is currently setup for COM1. //! If this is not correct, disconnect (Call->Disconnect) //! Open the File-Properties dialogue and select the correct COM port. //! -# Connect hyperterminal Call->Call //! and then start the 2837xD SCI echoback program execution. //! -# The program will print out a greeting and then ask you to //! enter a character which it will echo back to hyperterminal. //! //! \note If you are unable to open the .ht file, or you are using //! a different terminal, you can open a COM port with the following settings //! - Find correct COM port //! - Bits per second = 9600 //! - Date Bits = 8 //! - Parity = None //! - Stop Bits = 1 //! - Hardware Control = None //! //! \b Watch \b Variables \n //! - LoopCount - the number of characters sent //! //! \b External \b Connections \n //! Connect the SCI-A port to a PC via a transceiver and cable. //! - GPIO28 is SCI_A-RXD (Connect to Pin3, PC-TX, of serial DB9 cable) //! - GPIO29 is SCI_A-TXD (Connect to Pin2, PC-RX, of serial DB9 cable) //! // //########################################################################### // $TI Release: F2837xD Support Library v3.05.00.00 $ // $Release Date: Thu Oct 18 15:48:42 CDT 2018 $ // $Copyright: // Copyright (C) 2013-2018 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //########################################################################### // // Included Files // #include "F28x_Project.h" // // Globals // Uint16 LoopCount; // // Function Prototypes // void scia_echoback_init(void); void scia_fifo_init(void); void scia_xmit(int a); void scia_msg(char *msg); // // Main // void main(void) { Uint16 ReceivedChar; char *msg; // // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xD_SysCtrl.c file. // InitSysCtrl(); // // Step 2. Initialize GPIO: // This example function is found in the F2837xD_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // // For this example, only init the pins for the SCI-A port. // GPIO_SetupPinMux() - Sets the GPxMUX1/2 and GPyMUX1/2 register bits // GPIO_SetupPinOptions() - Sets the direction and configuration of the GPIOS // These functions are found in the F2837xD_Gpio.c file. // GPIO_SetupPinMux(9, GPIO_MUX_CPU1, 6); GPIO_SetupPinOptions(9, GPIO_INPUT, GPIO_PUSHPULL); GPIO_SetupPinMux(8, GPIO_MUX_CPU1, 6); GPIO_SetupPinOptions(8, GPIO_OUTPUT, GPIO_ASYNC); // // Step 3. Clear all __interrupts and initialize PIE vector table: // Disable CPU __interrupts // DINT; // // Initialize PIE control registers to their default state. // The default state is all PIE __interrupts disabled and flags // are cleared. // This function is found in the F2837xD_PieCtrl.c file. // InitPieCtrl(); // // Disable CPU __interrupts and clear all CPU __interrupt flags: // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the __interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in F2837xD_DefaultIsr.c. // This function is found in F2837xD_PieVect.c. // InitPieVectTable(); // // Step 4. User specific code: // LoopCount = 0; scia_fifo_init(); // Initialize the SCI FIFO scia_echoback_init(); // Initialize SCI for echoback unsigned char ch = 'a'; int n = 1; while(n) { scia_xmit(ch); DELAY_US(10000); } msg = "\r\n\n\nHello World!\0"; scia_msg(msg); msg = "\r\nYou will enter a character, and the DSP will echo it back! \n\0"; scia_msg(msg); for(;;) { msg = "\r\nEnter a character: \0"; scia_msg(msg); // // Wait for inc character // while(SciaRegs.SCIFFRX.bit.RXFFST == 0) { } // wait for empty state // // Get character // ReceivedChar = SciaRegs.SCIRXBUF.all; // // Echo character back // msg = " You sent: \0"; scia_msg(msg); scia_xmit(ReceivedChar); LoopCount++; } } // // scia_echoback_init - Test 1,SCIA DLB, 8-bit word, baud rate 0x000F, // default, 1 STOP bit, no parity // void scia_echoback_init() { // // Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function // SciaRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol SciaRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE SciaRegs.SCICTL2.all = 0x0003; SciaRegs.SCICTL2.bit.TXINTENA = 1; SciaRegs.SCICTL2.bit.RXBKINTENA = 1; // // SCIA at 9600 baud // @LSPCLK = 50 MHz (200 MHz SYSCLK) HBAUD = 0x02 and LBAUD = 0x8B. // @LSPCLK = 30 MHz (120 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x86. // SciaRegs.SCIHBAUD.all = 0x0002; SciaRegs.SCILBAUD.all = 0x008B; SciaRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset } // // scia_xmit - Transmit a character from the SCI // void scia_xmit(int a) { while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {} SciaRegs.SCITXBUF.all =a; } // // scia_msg - Transmit message via SCIA // void scia_msg(char * msg) { int i; i = 0; while(msg[i] != '\0') { scia_xmit(msg[i]); i++; } } // // scia_fifo_init - Initialize the SCI FIFO // void scia_fifo_init() { SciaRegs.SCIFFTX.all = 0xE040; SciaRegs.SCIFFRX.all = 0x2044; SciaRegs.SCIFFCT.all = 0x0; } // // End of file //
In this code I am just sending character 'a'
and I am receiving character like this,
my current setup is like this,
As you can see I have used level for conversion to 3.3 to 5V since I have device CP2102 USB to TTL converter.
I have observed level shifter which is working fine, scope when I tried transmitting '0' is like this,
yellow: output from launchpad (3.3V)
blue: output to CP2102 (5V)
Please guide me further!
Thanks in advance!
Akshay