Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello all,
i try to debug an apllication and experienced a difference in speed when i load the program to flash or RAM. My process is to set just one breakpoint at the begining of the main model. It gets executed through a software interrupt witha frequency of 10kHz. When i load the programm to flash and step through the programm with F5 (step into) the code needs about 1500 cycles to execute once. When i load the programm to RAM it and i step through it again with F5 it needs 2500 cycles. Is this possible?
Thanks!
Martin