Part Number: LAUNCHXL-F28379D
Hi,
I am currently using IMU9250 to get readings for Pitch via UAR with LaunchXL-F28379D. The output from this IMU is as follows:
<-8.24>
<-17.44> and so on..
I am able to get the output with basic sci loopback code. However, I want to use interrupts, as I need to call SCI within another protocol.
When I use the following code, I get no proper output but gibberish values.
What am I missing here?
//###########################################################################
//
// FILE: Example_2837xDSci_FFDLB_int.c
//
// TITLE: SCI Digital Loop Back with Interrupts.
//
//! \addtogroup cpu01_example_list
//! <h1>SCI Digital Loop Back with Interrupts (sci_loopback_interrupts)</h1>
//!
//! This program uses the internal loop back test mode of the peripheral.
//! Other then boot mode pin configuration, no other hardware configuration
//! is required. Both interrupts and the SCI FIFOs are used.
//!
//! A stream of data is sent and then compared to the received stream.
//! The SCI-A sent data looks like this: \n
//! 00 01 \n
//! 01 02 \n
//! 02 03 \n
//! .... \n
//! FE FF \n
//! FF 00 \n
//! etc.. \n
//! The pattern is repeated forever.
//!
//! \b Watch \b Variables \n
//! - \b sdataA - Data being sent
//! - \b rdataA - Data received
//! - \b rdata_pointA - Keep track of where we are in the data stream.
//! This is used to check the incoming data
//!
//
//###########################################################################
// $TI Release: F2837xD Support Library v3.05.00.00 $
// $Release Date: Thu Oct 18 15:48:42 CDT 2018 $
// $Copyright:
// Copyright (C) 2013-2018 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
//
// Defines
//
//
// Globals
//
Uint16 sdataA[2]; // Send data for SCI-A
Uint16 rdataA[2]; // Received data for SCI-A
Uint16 rdata_pointA; // Used for checking the received data
//
// Function Prototypes
//
interrupt void sciaTxFifoIsr(void);
interrupt void sciaRxFifoIsr(void);
void scia_fifo_init(void);
void error(void);
void scia_xmit(Uint16 a);
void scia_msg(Uint16 *msg);
//
// Main
//
void main(void)
{
Uint16 i;
Uint16 ReceivedChar;
Uint16 *msg;
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio();
//
// For this example, only init the pins for the SCI-A port.
// GPIO_SetupPinMux() - Sets the GPxMUX1/2 and GPyMUX1/2 register bits
// GPIO_SetupPinOptions() - Sets the direction and configuration of the GPIOS
// These functions are found in the F2837xD_Gpio.c file.
//
//
GPIO_SetupPinMux(43, GPIO_MUX_CPU1,15);
GPIO_SetupPinOptions(43, GPIO_INPUT, GPIO_PUSHPULL);
GPIO_SetupPinMux(42, GPIO_MUX_CPU1,15);
GPIO_SetupPinOptions(42, GPIO_OUTPUT, GPIO_ASYNC);
GPIO_SetupPinMux(19, GPIO_MUX_CPU1, 2);
GPIO_SetupPinOptions(19, GPIO_INPUT, GPIO_PUSHPULL);
GPIO_SetupPinMux(18, GPIO_MUX_CPU1, 2);
GPIO_SetupPinOptions(18, GPIO_OUTPUT, GPIO_ASYNC);
//
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.SCIB_RX_INT = &sciaRxFifoIsr;
// PieVectTable.SCIA_TX_INT = &sciaTxFifoIsr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize the Device Peripherals:
//
scia_fifo_init(); // Init SCI-A
//
// Step 5. User specific code, enable interrupts:
//
// Init send data. After each transmission this data
// will be updated for the next transmission
//
*msg =(char)ScibRegs.SCIRXBUF.all;
scia_msg(msg);
//
// Enable interrupts required for this example
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx1 = 1; // PIE Group 9, INT1
PieCtrlRegs.PIEIER9.bit.INTx2 = 1; // PIE Group 9, INT2
IER = 0x100; // Enable CPU INT
EINT;
//
// Step 6. IDLE loop. Just sit and loop forever (optional):
//
// for(;;);
}
//
// error - Function to halt debugger on error
//
void error(void)
{
asm(" ESTOP0"); // Test failed!! Stop!
for (;;);
}
//
// scia_xmit - Transmit a character from the SCI
//
void scia_xmit(Uint16 a)
{
while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {}
SciaRegs.SCITXBUF.all =a;
}
//
// scia_msg - Transmit message via SCIA
//
void scia_msg(Uint16 * msg)
{
int i;
i = 0;
while(msg[i] != '\n')
{
scia_xmit(msg[i]);
i++;
}
}
//
// sciaTxFifoIsr - SCIA Transmit FIFO ISR
//
/*interrupt void sciaTxFifoIsr(void)
{
Uint16 i;
for(i=0; i< 2; i++)
{
SciaRegs.SCITXBUF.all=sdataA[i]; // Send data
}
SciaRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear SCI Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}*/
//
// sciaRxFifoIsr - SCIA Receive FIFO ISR
//
interrupt void sciaRxFifoIsr(void)
{
Uint16 i;
i=(char)ScibRegs.SCIRXBUF.all; // Read data
scia_xmit(i);
ScibRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
//
// scia_fifo_init - Configure SCIA FIFO
//
void scia_fifo_init()
{
SciaRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.bit.TXINTENA = 1;
SciaRegs.SCICTL2.bit.RXBKINTENA = 1;
SciaRegs.SCIHBAUD.all =0x00; // 9600 baud @LSPCLK = 50MHz
//(200 MHz SYSCLK).
SciaRegs.SCILBAUD.all =0x0F;
//SciaRegs.SCICCR.bit.LOOPBKENA = 1; // Enable loop back
SciaRegs.SCIFFTX.all = 0xC022;
SciaRegs.SCIFFRX.all = 0x0022;
SciaRegs.SCIFFCT.all = 0x00;
SciaRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset
SciaRegs.SCIFFTX.bit.TXFIFORESET = 1;
SciaRegs.SCIFFRX.bit.RXFIFORESET = 1;
ScibRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.all = 0x0003;
ScibRegs.SCICTL2.bit.TXINTENA = 1;
ScibRegs.SCICTL2.bit.RXBKINTENA = 1;
ScibRegs.SCIHBAUD.all = 0x00;
ScibRegs.SCILBAUD.all = 0x0F;
ScibRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset
ScibRegs.SCIFFTX.all = 0xC022;//0xE040;
ScibRegs.SCIFFRX.all = 0x0022;//0x2044;
ScibRegs.SCIFFCT.all = 0x0;
ScibRegs.SCIFFTX.bit.TXFIFORESET = 1;
ScibRegs.SCIFFRX.bit.RXFIFORESET = 1;
}
//
// End of file
//