This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320F28379D: Problem with HwiHook example code in SYS/BIOS document

Part Number: TMS320F28379D

Tool/software: TI-RTOS

Hi,

I getting start with SYS/BIOS on F28379D. I read document   and try to follow it.

I found some problem when I test in HwiHook example code, it error when i compile.

- project file struct

- main.c

#include <xdc/std.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Timestamp.h>

#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/hal/Timer.h>
#include <ti/sysbios/hal/Hwi.h>

extern Timer_Handle myTimer;
volatile Bool myEnd2Flag = FALSE;
Int myHookSetId1, myHookSetId2;
Error_Block eb;

Error_init(&eb);

/* HookSet 1 functions */
/* ======== myRegister1 ========
 * invoked during Hwi module startup before main()
 * for each HookSet */
Void myRegister1(Int hookSetId){
    System_printf("myRegister1: assigned hookSet Id = %d\n", hookSetId);
    myHookSetId1 = hookSetId;
}

/* ======== myCreate1 ========
 * invoked during Hwi module startup before main()
 * for statically created Hwis */
Void myCreate1(Hwi_Handle hwi, Error_Block *eb){
    Ptr pEnv;
    pEnv = Hwi_getHookContext(hwi, myHookSetId1);
    /* pEnv should be 0 at this point. If not, there's a bug. */
    System_printf("myCreate1: pEnv = 0x%x, time = %d\n", pEnv, Timestamp_get32());
    Hwi_setHookContext(hwi, myHookSetId1, (Ptr)0xdead1);
}

/* ======== myBegin1 ========
 * invoked before Timer Hwi func */
Void myBegin1(Hwi_Handle hwi){
    Ptr pEnv;
    pEnv = Hwi_getHookContext(hwi, myHookSetId1);
    System_printf("myBegin1: pEnv = 0x%x, time = %d\n", pEnv, Timestamp_get32());
    Hwi_setHookContext(hwi, myHookSetId1, (Ptr)0xbeef1);
}

/* ======== myEnd1 ========
 * invoked after Timer Hwi func */
Void myEnd1(Hwi_Handle hwi){
    Ptr pEnv;
    pEnv = Hwi_getHookContext(hwi, myHookSetId1);
    System_printf("myEnd1: pEnv = 0x%x, time = %d\n", pEnv, Timestamp_get32());
    Hwi_setHookContext(hwi, myHookSetId1, (Ptr)0xc0de1);
}

/* HookSet 2 functions */
/* ======== myRegister2 ========
 * invoked during Hwi module startup before main
 * for each HookSet */
Void myRegister2(Int hookSetId){
    System_printf("myRegister2: assigned hookSet Id = %d\n", hookSetId);
    myHookSetId2 = hookSetId;
}

/* ======== myCreate2 ========
 * invoked during Hwi module startup before main
 * for statically created Hwis */
Void myCreate2(Hwi_Handle hwi, Error_Block *eb){
    Ptr pEnv;
    pEnv = Hwi_getHookContext(hwi, myHookSetId2);
    /* pEnv should be 0 at this point. If not, there's a bug. */
    System_printf("myCreate2: pEnv = 0x%x, time = %d\n", pEnv, Timestamp_get32());
    Hwi_setHookContext(hwi, myHookSetId2, (Ptr)0xdead2);
}

/* ======== myBegin2 ========
 * invoked before Timer Hwi func */
Void myBegin2(Hwi_Handle hwi){
    Ptr pEnv;
    pEnv = Hwi_getHookContext(hwi, myHookSetId2);
    System_printf("myBegin2: pEnv = 0x%x, time = %d\n", pEnv, Timestamp_get32());
    Hwi_setHookContext(hwi, myHookSetId2, (Ptr)0xbeef2);
}

/* ======== myEnd2 ========
 * invoked after Timer Hwi func */
Void myEnd2(Hwi_Handle hwi){
    Ptr pEnv;
    pEnv = Hwi_getHookContext(hwi, myHookSetId2);
    System_printf("myEnd2: pEnv = 0x%x, time = %d\n", pEnv, Timestamp_get32());
    Hwi_setHookContext(hwi, myHookSetId2, (Ptr)0xc0de2);
    myEnd2Flag = TRUE;
}

/* ======== myTimerFunc ========
 * Timer interrupt handler */
Void myTimerFunc(UArg arg){
    System_printf("Entering myTimerHwi\n");
}

/* ======== myTaskFunc ======== */
Void myTaskFunc(UArg arg0, UArg arg1){
    System_printf("Entering myTask.\n");
    Timer_start(myTimer);
    /* wait for timer interrupt and myEnd2 to complete */
    while (!myEnd2Flag) {
        ;
    }
    System_printf("myTask exiting ...\n");
}

/* ======== myIdleFunc ======== */
Void myIdleFunc(){
    System_printf("Entering myIdleFunc().\n");
    System_exit(0);
}

/* ======== main ======== */
Int main(Int argc, Char* argv[]){
    System_printf("Starting HwiHookExample...\n");
    BIOS_start();
    return (0);
}

/* ========== End of file ========= */

-app.cfg

/* pull in Timestamp to print time in hook functions */
xdc.useModule('xdc.runtime.Timestamp');

var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');

var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Task = xdc.useModule('ti.sysbios.knl.Task');


var Idle = xdc.useModule('ti.sysbios.knl.Idle');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
Idle.addFunc('&myIdleFunc');

/*
 * Uncomment this line to globally disable Asserts.
 * All modules inherit the default from the 'Defaults' module.  You
 * can override these defaults on a per-module basis using Module.common$. 
 * Disabling Asserts will save code space and improve runtime performance.
Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF;
 */

/*
 * Uncomment this line to keep module names from being loaded on the target.
 * The module name strings are placed in the .const section. Setting this
 * parameter to false will save space in the .const section.  Error and
 * Assert messages will contain an "unknown module" prefix instead
 * of the actual module name.
 */
Defaults.common$.namedModule = false;

/*
 * Minimize exit handler array in System.  The System module includes
 * an array of functions that are registered with System_atexit() to be
 * called by System_exit().
 */
System.maxAtexitHandlers = 4;       

/* 
 * Uncomment this line to disable the Error print function.  
 * We lose error information when this is disabled since the errors are
 * not printed.  Disabling the raiseHook will save some code space if
 * your app is not using System_printf() since the Error_print() function
 * calls System_printf().
Error.raiseHook = null;
 */

/* 
 * Uncomment this line to keep Error, Assert, and Log strings from being
 * loaded on the target.  These strings are placed in the .const section.
 * Setting this parameter to false will save space in the .const section.
 * Error, Assert and Log message will print raw ids and args instead of
 * a formatted message.
 */
Text.isLoaded = false;

/*
 * Uncomment this line to disable the output of characters by SysMin
 * when the program exits.  SysMin writes characters to a circular buffer.
 * This buffer can be viewed using the SysMin Output view in ROV.
 */
SysMin.flushAtExit = false;

/* 
 * The BIOS module will create the default heap for the system.
 * Specify the size of this default heap.
 */
BIOS.heapSize = 0x0;

/* System stack size (used by ISRs and Swis) */
Program.stack = 0x100;

/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x400;

/* 
 * Create and install logger for the whole system
 */
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 4;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;

System.SupportProxy = SysMin;

/*
 * Build a custom BIOS library.  The custom library will be smaller than the 
 * pre-built "instrumented" (default) and "non-instrumented" libraries.
 *
 * The BIOS.logsEnabled parameter specifies whether the Logging is enabled
 * within BIOS for this custom build.  These logs are used by the RTA and
 * UIA analysis tools.
 *
 * The BIOS.assertsEnabled parameter specifies whether BIOS code will
 * include Assert() checks.  Setting this parameter to 'false' will generate
 * smaller and faster code, but having asserts enabled is recommended for
 * early development as the Assert() checks will catch lots of programming
 * errors (invalid parameters, etc.)
 */
BIOS.logsEnabled = false;
BIOS.assertsEnabled = true;

BIOS.clockEnabled = false;

/* Create myTask with default task params */
var taskParams = new Task.Params();
Program.global.myTask = Task.create('&myTaskFunc', taskParams);

/* Create myTimer as source of Hwi */
var Timer = xdc.useModule('ti.sysbios.hal.Timer');
var timerParams = new Timer.Params();
timerParams.startMode = Timer.StartMode_USER;
timerParams.runMode = Timer.RunMode_ONESHOT;
timerParams.period = 1000; // 1ms
Program.global.myTimer = Timer.create(Timer.ANY, "&myTimerFunc", timerParams);

/* Define and add two Hwi HookSets
 * Notice, no deleteFxn is provided.
 */


/* Hook Set 1 */
Hwi.addHookSet({
	registerFxn: '&myRegister1',
	createFxn: '&myCreate1',
	beginFxn: '&myBegin1',
	endFxn: '&myEnd1',
});

/* Hook Set 2 */
Hwi.addHookSet({
	registerFxn: '&myRegister2',
	createFxn: '&myCreate2',
	beginFxn: '&myBegin2',
	endFxn: '&myEnd2',
});

-Error response

When I double click at error code it go to position error in main.c

These problem not found with SwiHook example code.

Thanks,

Thepnimit