Part Number: LAUNCHXL-F280049C
Tool/software: Code Composer Studio
Hi Team,
I tried to download example code using CCS v9.0.0.18 which has proper EMU Pack,
but still I can't download the code.
I got
The JTAG DR Integrity scan-test has succeeded.
message, when I used cJTAG 2pin mode in advanced setting of ccxml file,
still I can't download the code.
I got this on console.
CLA1_0: Error initializing emulator: (Error -2071 @ 0x0) Internal error: Missing or corrupt application file. Restart the application. If error persists, please report the error. (Emulation package 8.1.0.00005)
Best Regards,
Ted