Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
After the CLA program is changed from C to assembly, the CLA program _Cla1Task8 does not run when the CLA task 8 is triggered by asm(" IACK #0x0080") in the main function of C program, the same as the previous CLA C program. Referring to the example in the tI//c2000//c2000Ware_1_00_06_00// //device_support//f2837xd//examples//cpu1//cla_adc_fir32//cpu01//fir32.asm, the. sect "Cla1Prog" instruction has been added to the assembly file. In the initialization stage of C program, CLA program is copied to RAMLS3 specified by Cla1Prog.
Under the same condition of the main program, the previous CLA C program runs normally.
What causes it?