Part Number: TMDSHVMTRINSPIN
hi,
am using TMDSHVMTRINSPIN with a controller card F2806x , using the InstaFoc and the motor was ok for ID 409 volts, the max volt was on the VBUS was 157 v during testing, and maxmium speed i was able to reach its was 914 RPM , why cant i increase the speed more than that ? the motor is 12 pole , please help