Part Number: TMS320F28054M
Hi TI,
Under same acceleration, velocity and accuracy tolerance, why does FOC controlled motor is slower than PID controlled motor? And after 5 mins of running, motor tends to heat up.
I though FOC is more energy efficient and suppose to be faster because of higher torque capability.
I ran the speed tests using Trapezoidal motion profile, motor heats up within 5-6 minutes and it's 15-10% slower than PID controlled motor depending on the travelling ranges.
What are causes of slower speed and waste of heat. Wrong motor parameters? Or it simply just slower with same acceleration and velocity?
How can I at least match the speed of PID controlled motor with same accuracy tolerance?