Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
hey, I'm using the "MonoMtrServo_377s" example in ControlSuite for F2937xS, and i want to change it to work with the F29379D.
I was looking for GPIO pins used in this example for the SPI, and I saw that there are using a MUX for each GPIO pin as you can see in the image below : 
My question : can someone explain to me what is this MUX and why there are given it 15 ?
does 15 means that they are writing to register GPBMUX15 ??
here is the directory of the example I'm talking about : \controlSUITE\development_kits\TIDM-SERVO-LAUNCHXS\MonoMtrServo_377s_v1_00_00_00
the file that shown in the image is called "F2837xs_IO_assignment.h"
hope someone can help me.