Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: CONTROLSUITE
Dear TI Hello,
I want to measure the motor speed using CAP-1/Hall-1 already implemented in the TMDSHVMTRPFCKIT,
I am using a laser sensor, I connected the H-1 pin to the positive input '2' and GND to the pin '10',
The issue is even if i change the motor speed the Speed2.SpeedRpm remain unchanged 127!
Is there any other connection or jumpers I have to connect?
Thanks in advance,
Regards,
S.Tarik,