This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28379D: "FCL_379XL" controleSuite example

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: CONTROLSUITE, SFRA, DRV8305, BOOSTXL-DRV8305EVM

Tool/software: Code Composer Studio

I'm using the "FCL_379XL" example in ControleSuite, this example uses a dual motor with the DRV8305EVM.

for me, instead of using the motor I want to use 3 resistances connected to the DRV.

but in the program it's saying that in order to be able to measure the currents and the voltage, your need to set the motor1.RunMotor=STOP to motor1.RunMotor=RUN.

I tried doing it in the debbug session. but it reset to STOP itself instantly.

hope someone can help.

here is th path to example : controlSUITE\libs\app_libs\motor_control\libs\FCL_SFRA\v01_00_00_00\Examples\FCL_379XL