Part Number: TMDSHVMTRINSPIN
Hello all,
i have3 questions please , i have the HV kit TMDSHVMTRINSPIN :
1-the speed that show for the BLDC motor on the InstaFOC or Motion are not the same as the one i measure with tachometer the real speed is 1/3 of the one shown on motion or FOC
2-how can i control what frequency i can run the motor at ? for example at 400Hz , what setting do i change in the InstaFOC or Motion ?
3-if i use one of the VFD it run the same motor at 400Hz the BLDC senso rless motor run at 1000 RPM but with the default setting of the HV kit the motor run at 450 RPM , how can change the operating Frequency ?