This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: Problem about bootloader

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

Hi

       I have a trouble recently when I develop a project using 28377. I try to  run my app in the sram load from flash, acourding to "SPRAAU8A" apprach, add the file "DSP28xxx_SectionCopy_nonBIOS.asm"  and change the file "F2837xS_CodeStartBranch.asm" instead of the "DSP28xxx_CodeStartBranch.asm". but afer build project and load, the CCS halt at 0x3fe493 before jump to main(). so can anyone help me?

     by the way, my app is run correctly when load to ram and load to flash that not use bootloader.

"DSP28xxx_CodeStartBranch.asm" content below: 

WD_DISABLE .set 1                 ;set to 1 to disable WD, else set to 0

.ref copy_sections
.global code_start

***********************************************************************
* Function: codestart section
*
* Description: Branch to code starting point
***********************************************************************

.sect "codestart"

code_start:
.if WD_DISABLE == 1
LB wd_disable                   ;Branch to watchdog disable code
.else
LB copy_sections                 ;Branch to copy_sections 
.endif

;end codestart section

***********************************************************************
* Function: wd_disable
*
* Description: Disables the watchdog timer
***********************************************************************
.if WD_DISABLE == 1

.text
wd_disable:
SETC OBJMODE             ;    Set OBJMODE for 28x object code
EALLOW                            ;           Enable EALLOW protected register access
MOVZ DP, #7029h>>6                ;              Set data page for WDCR register
MOV @7029h, #0068h         ;           Set WDDIS bit in WDCR to disable WD
EDIS                                           ;Disable EALLOW protected register access
LB copy_sections ;Branch to copy_sections

.endif

 "DSP28xxx_SectionCopy_nonBIOS.asm" content below:

.ref _c_int00
.global copy_sections
.global _cinit_loadstart, _cinit_runstart, _cinit_size
.global _const_loadstart, _const_runstart, _const_size
.global _econst_loadstart, _econst_runstart, _econst_size
.global _pinit_loadstart, _pinit_runstart, _pinit_size
.global _switch_loadstart, _switch_runstart, _switch_size
.global _text_loadstart, _text_runstart, _text_size

***********************************************************************
* Function: copy_sections
*
* Description: Copies initialized sections from flash to ram
***********************************************************************

.sect "copysections"

copy_sections:


MOVL XAR5,#_cinit_size                           ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_cinit_loadstart               ; Store Load Starting Address in XAR6
MOVL XAR7,#_cinit_runstart                    ; Store Run Address in XAR7
LCR copy                                                    ; Branch to Copy

MOVL XAR5,#_const_size                         ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_const_loadstart                ; Store Load Starting Address in XAR6
MOVL XAR7,#_const_runstart                 ; Store Run Address in XAR7
LCR copy                                                     ; Branch to Copy

MOVL XAR5,#_econst_size                     ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_econst_loadstart             ; Store Load Starting Address in XAR6
MOVL XAR7,#_econst_runstart               ; Store Run Address in XAR7
LCR copy                                                     ; Branch to Copy

MOVL XAR5,#_pinit_size                         ; Store Section Size in XAR5
MOVL ACC,@XAR5                                   ; Move Section Size to ACC
MOVL XAR6,#_pinit_loadstart                 ; Store Load Starting Address in XAR6
MOVL XAR7,#_pinit_runstart                   ; Store Run Address in XAR7
LCR copy                                                       ; Branch to Copy

MOVL XAR5,#_switch_size                     ; Store Section Size in XAR5
MOVL ACC,@XAR5                                  ; Move Section Size to ACC
MOVL XAR6,#_switch_loadstart              ; Store Load Starting Address in XAR6
MOVL XAR7,#_switch_runstart               ; Store Run Address in XAR7
LCR copy                                                      ; Branch to Copy

MOVL XAR5,#_text_size                               ; Store Section Size in XAR5
MOVL ACC,@XAR5                                    ; Move Section Size to ACC
MOVL XAR6,#_text_loadstart                    ; Store Load Starting Address in XAR6
MOVL XAR7,#_text_runstart                     ; Store Run Address in XAR7
LCR copy                                                   ; Branch to Copy


LB _c_int00                                                 ; Branch to start of boot.asm in RTS library

copy: 
B return,EQ                                                ; Return if ACC is Zero (No section to copy)

SUBB ACC,#1

RPT AL                                                        ; Copy Section From Load Address to
|| PWRITE *XAR7, *XAR6++                    ; Run Address

return:
LRETR                                                        ; Return

.end

CMD content below:


MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS : origin = 0x008000, length = 0x003000


RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE                  /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x07E000                 /* on-chip Flash */

PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

BOOT_RSVD : origin = 0x000002, length = 0x000120                     /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400                            /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800

RAMGS : origin = 0x00C000, length = 0x010000
}


SECTIONS
{
/* Allocate program areas: */

codestart : > BEGIN PAGE = 0, ALIGN(4)
copysections : > FLASHB PAGE = 0, ALIGN(4)

/*** Initialized Sections ***/
.cinit : LOAD = FLASHB, PAGE = 0            /* can be ROM */
RUN = RAMLS, PAGE = 0                          /* must be CSM secured RAM */
LOAD_START(_cinit_loadstart),
RUN_START(_cinit_runstart),
SIZE(_cinit_size)

.const : LOAD = FLASHB, PAGE = 0                 /* can be ROM */
RUN = RAMLS, PAGE = 0                              /* must be CSM secured RAM */
LOAD_START(_const_loadstart),
RUN_START(_const_runstart),
SIZE(_const_size)

.econst : LOAD = FLASHB, PAGE = 0                      /* can be ROM */
RUN = RAMLS, PAGE = 0                                      /* must be CSM secured RAM */
LOAD_START(_econst_loadstart),
RUN_START(_econst_runstart),
SIZE(_econst_size)

.pinit : LOAD = FLASHB, PAGE = 0                      /* can be ROM */
RUN = RAMLS, PAGE = 0                                         /* must be CSM secured RAM */
LOAD_START(_pinit_loadstart),
RUN_START(_pinit_runstart),
SIZE(_pinit_size)

.switch : LOAD = FLASHB, PAGE = 0                            /* can be ROM */
RUN = RAMLS, PAGE = 0                                            /* must be CSM secured RAM */
LOAD_START(_switch_loadstart),
RUN_START(_switch_runstart),
SIZE(_switch_size)

.text : LOAD = FLASHB, PAGE = 0                                   /* can be ROM */
RUN = RAMLS, PAGE = 0                                             /* must be CSM secured RAM */
LOAD_START(_text_loadstart),
RUN_START(_text_runstart),
SIZE(_text_size)


/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAMGS PAGE = 1
.esysmem : > RAMGS PAGE = 1

/* Initalized sections go in Flash */

.reset : > RESET, PAGE = 0, TYPE = DSECT                   /* not used, */

}

  • Hi Katta

           thanks for your reply, I have refered the 884720, the problem is not the same as mine. 

          The first is My hardware, emulator and App work well, since my app runs correctly boot to RAM using "28377S_RAM_lnk.cmd".

         also my app runs correctly boot to flash using "2837xS_Generic_FLASH_lnk.cmd"  with certain sections copy to ram.

         but when I try to copy the entire app from flash to ram, after build and load, ccs halt at 0x3fe493, then press run buton, loop at 0x3fe493. 

         seems jump to ITRAP interrupt and dead loop. I don't know why?

         

  • Hi,

    Can you please tell me how many extra words were added with your change in the example for .TI.ramfunc?

    If the size exceeds the size of RAMLS0 i.e. 0x800, combine RAMs. For ex:-

    .TI.ramfunc : {} LOAD = FLASHD,
    RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,

    Modify it to
    .TI.ramfunc : {} LOAD = FLASHD,
    RUN = RAMLS03,

    where RAMLS03 : origin = 0x008000, length = 0x002000

    Please try with this change.

    Thanks,
    Katta