Hi expert,
My customer has an application in which F280049 is inside a rotation machine. In this case, F280049 works in high ambient temperature so they need a functionality to monitor temperature (ambient or junction) to protect F280049 when temperature is too high (in some fault state temperature will rise).
We noticed that internal temperature sensor has a typical accuracy of +- 15 degrees centigrade which will not do a precise protection.
Could we put a surface mount NTC/PTC on PCB board to monitor ambient temperature and indirectly project the MCU? If we could, how?
Thanks
Sheldon