This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Using CAN to update FW

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

I'm looking for code examples or project examples of how to use the CAN bootloader on F28377D and F28069.

The goal is to use the CAN bus to update firmware on these devices.

  • Hello

    We don't specifically have an example that uses the CAN bootloader. In C2000Ware, you can find the CAN bootloader source code. You'll use the C2000 HEX utility to convert the project to the necessary HEX format required by the bootloader. Depending on what the platform is that is sending the program, you'll need a CAN adapter such as PCAN to connect a PC to a CAN network.

    Best regards
    Chris