Hi,
in F280049 datasheet it says "Analog input pins with PGAx_OUTF" should be no connect or Tie to VSSA through 4.7-kΩ or larger resistor.
But I can't find any pin name contains OUTF.
Analog input pins (except for DACx_OUT and PGAx_OUTF) should be No Connect • or Tie to VSSA • or Tie to VSSA through resistor, does it apply to PGA_IN?
And for 100pin F280049, PIN 61 is muxed between TDO and LINA_TX, PIN63 is muxed between TDI and LINA_RX, so is it possible that we use PIN61 and 63 as JTAG at the same time as LIN communication interface? Are there anything need to take special consideration to do so?