Hi There,
I'm reviewing the above schematic design and I note that the current sensor output is being connected to 4 ADC pins:
| Signal Name | HSEC-180 Pin | MCU Pin ID | MCU Pin | 
| I.inv(1) | 15 | ADC-A2 | U2 | 
| I.inv(2) | 18 | ADC-B2 | V3 | 
| I.inv(3) | 28 | ADC-D0 | T5 | 
| I.inv(4) | 31 | ADC-C2 | R3 | 
As I am looking at porting to F28377S (100 pin) I only have a limited number of ADCs and was wondering if I do need the last 2 ADC inputs? or could rewrite the code to point to the first two ADCs instead?
Thanks in advance
Robin