How many PWM channels of TMS320F28069 are HRPWM capable?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks Himanshu.
I read in the datasheet that only 8 out of 16 channels( only ePWMxAs ) are hrpwm capable. Can I still use the B channels to generate the complementary signals to drive half-bridge transistors. If yes, then in a sense the B channels become hrpwm capable too (since both A and B have the same resolution now). Please clarify and point out if I am missing something here.
Hi,
Yes you point seems valid. Please refer to TRM for more info, I am attaching the relevant screenshot
---------------------------------------------------------------------------------------------------
If a post answers your question, please mark it with the "verify answer" button.
Regards
Himanshu