Other Parts Discussed in Thread: C2000WARE
Hi,
Looking at the 180-pin HSEC card pinout .PDF file (TMDSCNCD28377D_180cCARD_pinout_R1_3.pdf), within the C2000ware set of documents, I am seeing that on the 60 position (120-pin) connector, "pin 1" is defined as being on the "shorter" portion of the connector (that is, the side of the gap with 28 positions). The same also goes with the docking station pinout.
This is inconsistent with pin 1 designation on the part used in the BOM for the card edge connector on the docking station (HSEC8-160-01-L-DV-A-BL), Where pin-1 seems to be on the "bigger" portion of the connector (that is, the side of the gap with 32 positions.
Would it be possible to get confirmation on this observation?
Thanks!