Part Number: TMS320F28335
Tool/software: Code Composer Studio
Sir,
We are using TMS320F28335 DSP board with CCS 6.0.0 for the FOC of PMSM with specification - 75VDC, 8000RPM.
We are implementing FOC of PMSM on the basis of the pdfs http://www.ti.com/lit/an/sprabz0/sprabz0.pdf and http://www.ti.com/lit/an/sprabq3/sprabq3.pdf.
1. We have done the first level incremental build of FOC as per the pdf with our motor specifications, we have got the SVPWM output on the CRO and verified with the above pdfs. But can you please tell the settings needed for getting the waveform outputs on the watch window as shown in the pdfs?
2. We just tried the second level incremental build of FOC as per the pdf to run the motor at 400rpm by giving 25VDC. But, the current feedback we got from the CRO is having distortions at the peak points. I have attached its image with this. Can you please help us to find out what is the error?