This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28379D: CLA and Flash linker file

Part Number: LAUNCHXL-F28379D


Tool/software: Code Composer Studio

Hello TI people,
Am working on TMS320F28379D Delfino launchpad. I have managed to run a simple code on CLA processor in parallel with CPU1 using RAM linker file. For the time being i have migrated to Flash linker file (provided from CC2000ware_x_x_x) but the code is no longer working. Sure, I have defined the CPU1,  FLASH macro and CLA_C in predefined symbols that reside in project properties.
Am here for any suggestion.

I posted the same question on this thread "e2e.ti.com/.../792762" but no one replay i got and it was useless.  

best regards
Hosam