This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: IEC60730 for F28374s

Part Number: TMS320F28374S

Hi Team,

  From C2000 Safety Enabler file, there is no F28374s IEC60730 related description,  Could you kindly help give comments for schedule of IEC60730?

Best Regards

Benjamin

  • Benjamin,

    The diagnostics provided in the SafeTI Software Diagnostic Library (SDL) for F2837xS/D and F2807x can be mapped to IEC60730 Class-C diagnostic methods.  The mapping of library APIs to Class-C diagnostic methods is documented in the C2000™ SafeTI™ Diagnostic Library Software Safety Manual (SPRUIH0).  This manual is included in the doc/ directory of the SDL.  While the libraries have not been specifically assessed against IEC60730 by a 3rd party, the contentment of the libraries enable TI customers to achieve compliance to IEC60730.  

    Regards,

    Lori

  • Lori,
    My understanding is that TI can't provide IEC60730 assessment report on F2837xS/D at this moment, customer need to using the SDL & safety manual to support their IEC60730 assessment.

    Noticed with lots of thanks.

    Best Regards
    Benjamin
  • Benjamin Zhou said:
    TI can't provide IEC60730 assessment report on F2837xS/D at this moment, customer need to using the SDL & safety manual to support their IEC60730 assessment.

    Benjamin,

    This is correct with one clarification.  There is no plan to have the library assessed specifically against IEC60730.

    Regards

    Lori