Tool/software: Code Composer Studio
Hello Guys:
I am working on TMS320F28377S platform for a instruments project, I have selected QFP176 package for this application, In my system there is a FPGA working with the DSP, I need EMIF1 port of DSP to connect with FPGA, So I have met a question which is EM1D12 (I/O) function is also mapped GPIO72 (Boot pin)function, If device boot from Flash I need set the boot mode as the get mode It means GPIO72 need pull up to VCC3.3V with a 1K resister, But when I use EM1 port as the data communication port I can not hold the D12 in 3.3V, So are there any way to work around this issue???
Thanks
RZ