This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: The application code which is download after the bootloader code will cover the bootloader code, how to avoid that?

Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH

Tool/software: Code Composer Studio

Dears,

     F28335 is used for the motor driver, there are 2 parts of the code, one is the bootloader code, the other is the application code.

the bootloader code was programed into DSP first, and then the application code will be programed. If the later application was download in a CAN bus, the later code will not cover the bootloader code, but if the application code was programed in a JTAG way, the later code will cover the bootloader code, how to avoid this covering when using a JTAG way to down load the application code after the bootloader code was download?

      Finally, is there a better way to solve this issue? for example, how can I down load the bootloader code and application code in one time rather than separately?

    Thanks.