This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team:
Below is the original path of the code:
I use the official routine to test the lin module on F280049. But the code was stop at the below position:
It is caused by the failure to enter the corresponding interrupt, But why it didn't enter the interrupt? Below is the interrupt function:
The LIN pins used are the following two:
Best regards
Dear Sir/Madam,
We are unable to replicate the issue you have reported here. So we will need some additional details in order to help you.
Have you made any changes to the example provided in C2000Ware? If so, can you please provide a summary of those changes.
Thanks,
Krishna
Dear Krishna
I just changed two pins of LIN. But I tested the same phenomenon before changing.
Best regards
Dear Sir/Madam,
Please restore to the factory configuration and let us know if you see normal operation. If you do, then we can debug how the change may be impacting functionality.
Cheers!
Krishna